2.18.2 Incorrect Periodic Daily Event at 23:59:58

Periodic Delay Event needs to be asserted at the end of the prescaler period to be generated on the last second of the day. As the prescaler overflow does not qualify the Periodic Delay Event, the event is generated at the beginning of the prescaler period, hence, one second earlier than specified.

Work Around:

The user application may wait 1 sec to process the periodic daily event.

Affected Silicon Revisions

PIC32CX1012BZ25048/WBZ451/WBZ451H
A0A2
XX
PIC32CX1012BZ24032/WBZ450
A2
X