39.6.2.4 DMA Dynamic Linking of a New Transfer Descriptor
- Write the new descriptor structure in the system memory.
- Write the address of the new structure in the CHXHEAD register.
- Add the new structure to the queue of descriptors by writing one to the A2QEN field of the CHXCHER register.
- The new descriptor is added to the queue on the next frame.
- An interrupt is raised if unmasked, when the head descriptor structure has been loaded by the DMA channel.