1.4.3.17 SYS_WIFI_Tasks Function

C

uint8_t SYS_WIFI_Tasks ( SYS_MODULE_OBJ object)

Summary

Maintains the Wi-Fi System tasks and functionalities.

Description

This function is used to run the various tasks and functionalities of Wi-Fi system service.

Precondition

The SYS_WIFI_Initialize function should have been called before calling this function.

Parameters

ParamDescription
objectSYS WIFI object handle, returned from SYS_WIFI_Initialize

Returns

return SYS_WIFI_STATUS if client provided object is valid, else return SYS_WIFI_OBJ_INVALID.

Example

if (SYS_WIFI_OBJ_INVALID != SYS_WIFI_Tasks (sysObj.syswifi))
{
    
}

Remarks

If the Wi-Fi system service is enabled using MHC, then auto generated code will take care of system task execution.