4.153.75 size_t strlen_P
size_t strlen_P(const char *s)
The strlen_P() function is similar to strlen(), except that src is a pointer to a string in program space.
Remember:
The strlen_P() function returns the number of characters in src.
Note:
strlen_P() is implemented as an inline function in the avr/pgmspace.h header file, which will check if the length of the string is a constant and known at compile time. If it is not known at compile time, the macro will issue a call to __strlen_P() which will then calculate the length of the string as normal.