4.18.24 boot.h
/* Copyright (c) 2002,2003,2004,2005,2006,2007,2008,2009 Eric B. Weddington
All rights reserved.
Redistribution and use in source and binary forms, with or without
modification, are permitted provided that the following conditions are met:
* Redistributions of source code must retain the above copyright
notice, this list of conditions and the following disclaimer.
* Redistributions in binary form must reproduce the above copyright
notice, this list of conditions and the following disclaimer in
the documentation and/or other materials provided with the
distribution.
* Neither the name of the copyright holders nor the names of
contributors may be used to endorse or promote products derived
from this software without specific prior written permission.
THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE
IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE
ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE
LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR
CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF
SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS
INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN
CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE)
ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
POSSIBILITY OF SUCH DAMAGE. */
/* $Id$ */
#ifndef _AVR_BOOT_H_
#define _AVR_BOOT_H_ 1
/** \file */
/** \defgroup avr_boot <avr/boot.h>: Bootloader Support Utilities
\code
#include <avr/io.h>
#include <avr/boot.h>
\endcode
The macros in this module provide a C language interface to the
bootloader support functionality of certain AVR processors. These
macros are designed to work with all sizes of flash memory.
Global interrupts are not automatically disabled for these macros. It
is left up to the programmer to do this. See the code example below.
Also see the processor datasheet for caveats on having global interrupts
enabled during writing of the Flash.
\note Not all AVR processors provide bootloader support. See your
processor datasheet to see if it provides bootloader support.
\todo From email with Marek: On smaller devices (all except ATmega64/128),
__SPM_REG is in the I/O space, accessible with the shorter "in" and "out"
instructions - since the boot loader has a limited size, this could be an
important optimization.
\par API Usage Example
The following code shows typical usage of the boot API.
\code
#include <inttypes.h>
#include <avr/interrupt.h>
#include <avr/pgmspace.h>
void boot_program_page (uint32_t page, uint8_t *buf)
{
uint16_t i;
uint8_t sreg;
// Disable interrupts.
sreg = SREG;
cli();
eeprom_busy_wait ();
boot_page_erase (page);
boot_spm_busy_wait (); // Wait until the memory is erased.
for (i=0; i<SPM_PAGESIZE; i+=2)
{
// Set up little-endian word.
uint16_t w = *buf++;
w += (*buf++) << 8;
boot_page_fill (page + i, w);
}
boot_page_write (page); // Store buffer in flash page.
boot_spm_busy_wait(); // Wait until the memory is written.
// Reenable RWW-section again. We need this if we want to jump back
// to the application after bootloading.
boot_rww_enable ();
// Re-enable interrupts (if they were ever enabled).
SREG = sreg;
}\endcode */
#include <avr/eeprom.h>
#include <avr/io.h>
#include <inttypes.h>
#include <limits.h>
/* Check for SPM Control Register in processor. */
#if defined (SPMCSR)
# define __SPM_REG SPMCSR
#else
# if defined (SPMCR)
# define __SPM_REG SPMCR
# else
# error AVR processor does not provide bootloader support!
# endif
#endif
/* Check for SPM Enable bit. */
#if defined(SPMEN)
# define __SPM_ENABLE SPMEN
#elif defined(SELFPRGEN)
# define __SPM_ENABLE SELFPRGEN
#else
# error Cannot find SPM Enable bit definition!
#endif
/** \ingroup avr_boot
\def BOOTLOADER_SECTION
Used to declare a function or variable to be placed into a
new section called .bootloader. This section and its contents
can then be relocated to any address (such as the bootloader
NRWW area) at link-time. */
#define BOOTLOADER_SECTION __attribute__ ((section (".bootloader")))
#ifndef __DOXYGEN__
/* Create common bit definitions. */
#ifdef ASB
#define __COMMON_ASB ASB
#else
#define __COMMON_ASB RWWSB
#endif
#ifdef ASRE
#define __COMMON_ASRE ASRE
#else
#define __COMMON_ASRE RWWSRE
#endif
/* Define the bit positions of the Boot Lock Bits. */
#define BLB12 5
#define BLB11 4
#define BLB02 3
#define BLB01 2
#endif /* __DOXYGEN__ */
/** \ingroup avr_boot
\def boot_spm_interrupt_enable()
Enable the SPM interrupt. */
#define boot_spm_interrupt_enable() (__SPM_REG |= (uint8_t)_BV(SPMIE))
/** \ingroup avr_boot
\def boot_spm_interrupt_disable()
Disable the SPM interrupt. */
#define boot_spm_interrupt_disable() (__SPM_REG &= (uint8_t)~_BV(SPMIE))
/** \ingroup avr_boot
\def boot_is_spm_interrupt()
Check if the SPM interrupt is enabled. */
#define boot_is_spm_interrupt() (__SPM_REG & (uint8_t)_BV(SPMIE))
/** \ingroup avr_boot
\def boot_rww_busy()
Check if the RWW section is busy. */
#define boot_rww_busy() (__SPM_REG & (uint8_t)_BV(__COMMON_ASB))
/** \ingroup avr_boot
\def boot_spm_busy()
Check if the SPM instruction is busy. */
#define boot_spm_busy() (__SPM_REG & (uint8_t)_BV(__SPM_ENABLE))
/** \ingroup avr_boot
\def boot_spm_busy_wait()
Wait while the SPM instruction is busy. */
#define boot_spm_busy_wait() do{}while(boot_spm_busy())
#ifndef __DOXYGEN__
#define __BOOT_PAGE_ERASE (_BV(__SPM_ENABLE) | _BV(PGERS))
#define __BOOT_PAGE_WRITE (_BV(__SPM_ENABLE) | _BV(PGWRT))
#define __BOOT_PAGE_FILL _BV(__SPM_ENABLE)
#define __BOOT_RWW_ENABLE (_BV(__SPM_ENABLE) | _BV(__COMMON_ASRE))
#if defined(BLBSET)
#define __BOOT_LOCK_BITS_SET (_BV(__SPM_ENABLE) | _BV(BLBSET))
#elif defined(RFLB) /* Some devices have RFLB defined instead of BLBSET. */
#define __BOOT_LOCK_BITS_SET (_BV(__SPM_ENABLE) | _BV(RFLB))
#endif
#define __boot_page_fill_normal(address, data) \
(__extension__({ \
__asm__ __volatile__ \
( \
"movw r0, %3\n\t" \
"sts %0, %1\n\t" \
"spm\n\t" \
"clr r1\n\t" \
: \
: "i" (_SFR_MEM_ADDR(__SPM_REG)), \
"r" ((uint8_t)(__BOOT_PAGE_FILL)), \
"z" ((uint16_t)(address)), \
"r" ((uint16_t)(data)) \
: "r0" \
); \
}))
#define __boot_page_fill_alternate(address, data)\
(__extension__({ \
__asm__ __volatile__ \
( \
"movw r0, %3\n\t" \
"sts %0, %1\n\t" \
"spm\n\t" \
".word 0xffff\n\t" \
"nop\n\t" \
"clr r1\n\t" \
: \
: "i" (_SFR_MEM_ADDR(__SPM_REG)), \
"r" ((uint8_t)(__BOOT_PAGE_FILL)), \
"z" ((uint16_t)(address)), \
"r" ((uint16_t)(data)) \
: "r0" \
); \
}))
#define __boot_page_fill_extended(address, data) \
(__extension__({ \
__asm__ __volatile__ \
( \
"movw r0, %4\n\t" \
"movw r30, %A3\n\t" \
"sts %1, %C3\n\t" \
"sts %0, %2\n\t" \
"spm\n\t" \
"clr r1\n\t" \
: \
: "i" (_SFR_MEM_ADDR(__SPM_REG)), \
"i" (_SFR_MEM_ADDR(RAMPZ)), \
"r" ((uint8_t)(__BOOT_PAGE_FILL)), \
"r" ((uint32_t)(address)), \
"r" ((uint16_t)(data)) \
: "r0", "r30", "r31" \
); \
}))
#define __boot_page_erase_normal(address) \
(__extension__({ \
__asm__ __volatile__ \
( \
"sts %0, %1\n\t" \
"spm\n\t" \
: \
: "i" (_SFR_MEM_ADDR(__SPM_REG)), \
"r" ((uint8_t)(__BOOT_PAGE_ERASE)), \
"z" ((uint16_t)(address)) \
); \
}))
#define __boot_page_erase_alternate(address) \
(__extension__({ \
__asm__ __volatile__ \
( \
"sts %0, %1\n\t" \
"spm\n\t" \
".word 0xffff\n\t" \
"nop\n\t" \
: \
: "i" (_SFR_MEM_ADDR(__SPM_REG)), \
"r" ((uint8_t)(__BOOT_PAGE_ERASE)), \
"z" ((uint16_t)(address)) \
); \
}))
#define __boot_page_erase_extended(address) \
(__extension__({ \
__asm__ __volatile__ \
( \
"movw r30, %A3\n\t" \
"sts %1, %C3\n\t" \
"sts %0, %2\n\t" \
"spm\n\t" \
: \
: "i" (_SFR_MEM_ADDR(__SPM_REG)), \
"i" (_SFR_MEM_ADDR(RAMPZ)), \
"r" ((uint8_t)(__BOOT_PAGE_ERASE)), \
"r" ((uint32_t)(address)) \
: "r30", "r31" \
); \
}))
#define __boot_page_write_normal(address) \
(__extension__({ \
__asm__ __volatile__ \
( \
"sts %0, %1\n\t" \
"spm\n\t" \
: \
: "i" (_SFR_MEM_ADDR(__SPM_REG)), \
"r" ((uint8_t)(__BOOT_PAGE_WRITE)), \
"z" ((uint16_t)(address)) \
); \
}))
#define __boot_page_write_alternate(address) \
(__extension__({ \
__asm__ __volatile__ \
( \
"sts %0, %1\n\t" \
"spm\n\t" \
".word 0xffff\n\t" \
"nop\n\t" \
: \
: "i" (_SFR_MEM_ADDR(__SPM_REG)), \
"r" ((uint8_t)(__BOOT_PAGE_WRITE)), \
"z" ((uint16_t)(address)) \
); \
}))
#define __boot_page_write_extended(address) \
(__extension__({ \
__asm__ __volatile__ \
( \
"movw r30, %A3\n\t" \
"sts %1, %C3\n\t" \
"sts %0, %2\n\t" \
"spm\n\t" \
: \
: "i" (_SFR_MEM_ADDR(__SPM_REG)), \
"i" (_SFR_MEM_ADDR(RAMPZ)), \
"r" ((uint8_t)(__BOOT_PAGE_WRITE)), \
"r" ((uint32_t)(address)) \
: "r30", "r31" \
); \
}))
#define __boot_rww_enable() \
(__extension__({ \
__asm__ __volatile__ \
( \
"sts %0, %1\n\t" \
"spm\n\t" \
: \
: "i" (_SFR_MEM_ADDR(__SPM_REG)), \
"r" ((uint8_t)(__BOOT_RWW_ENABLE)) \
); \
}))
#define __boot_rww_enable_alternate() \
(__extension__({ \
__asm__ __volatile__ \
( \
"sts %0, %1\n\t" \
"spm\n\t" \
".word 0xffff\n\t" \
"nop\n\t" \
: \
: "i" (_SFR_MEM_ADDR(__SPM_REG)), \
"r" ((uint8_t)(__BOOT_RWW_ENABLE)) \
); \
}))
/* From the mega16/mega128 data sheets (maybe others):
Bits by SPM To set the Boot Loader Lock bits, write the desired data to
R0, write "X0001001" to SPMCR and execute SPM within four clock cycles
after writing SPMCR. The only accessible Lock bits are the Boot Lock bits
that may prevent the Application and Boot Loader section from any
software update by the MCU.
If bits 5..2 in R0 are cleared (zero), the corresponding Boot Lock bit
will be programmed if an SPM instruction is executed within four cycles
after BLBSET and SPMEN (or SELFPRGEN) are set in SPMCR. The Z-pointer is
don't care during this operation, but for future compatibility it is
recommended to load the Z-pointer with $0001 (same as used for reading the
Lock bits). For future compatibility It is also recommended to set bits 7,
6, 1, and 0 in R0 to 1 when writing the Lock bits. When programming the
Lock bits the entire Flash can be read during the operation. */
#define __boot_lock_bits_set(lock_bits) \
(__extension__({ \
uint8_t value = (uint8_t)(~(lock_bits)); \
__asm__ __volatile__ \
( \
"ldi r30, 1\n\t" \
"ldi r31, 0\n\t" \
"mov r0, %2\n\t" \
"sts %0, %1\n\t" \
"spm\n\t" \
: \
: "i" (_SFR_MEM_ADDR(__SPM_REG)), \
"r" ((uint8_t)(__BOOT_LOCK_BITS_SET)), \
"r" (value) \
: "r0", "r30", "r31" \
); \
}))
#define __boot_lock_bits_set_alternate(lock_bits) \
(__extension__({ \
uint8_t value = (uint8_t)(~(lock_bits)); \
__asm__ __volatile__ \
( \
"ldi r30, 1\n\t" \
"ldi r31, 0\n\t" \
"mov r0, %2\n\t" \
"sts %0, %1\n\t" \
"spm\n\t" \
".word 0xffff\n\t" \
"nop\n\t" \
: \
: "i" (_SFR_MEM_ADDR(__SPM_REG)), \
"r" ((uint8_t)(__BOOT_LOCK_BITS_SET)), \
"r" (value) \
: "r0", "r30", "r31" \
); \
}))
#endif /* __DOXYGEN__ */
/*
Reading lock and fuse bits:
Similarly to writing the lock bits above, set BLBSET and SPMEN (or
SELFPRGEN) bits in __SPMREG, and then (within four clock cycles) issue an
LPM instruction.
Z address: contents:
0x0000 low fuse bits
0x0001 lock bits
0x0002 extended fuse bits
0x0003 high fuse bits
Sounds confusing, doesn't it?
Unlike the macros in pgmspace.h, no need to care for non-enhanced
cores here as these old cores do not provide SPM support anyway.
*/
/** \ingroup avr_boot
\def GET_LOW_FUSE_BITS
address to read the low fuse bits, using boot_lock_fuse_bits_get
*/
#define GET_LOW_FUSE_BITS (0x0000)
/** \ingroup avr_boot
\def GET_LOCK_BITS
address to read the lock bits, using boot_lock_fuse_bits_get
*/
#define GET_LOCK_BITS (0x0001)
/** \ingroup avr_boot
\def GET_EXTENDED_FUSE_BITS
address to read the extended fuse bits, using boot_lock_fuse_bits_get
*/
#define GET_EXTENDED_FUSE_BITS (0x0002)
/** \ingroup avr_boot
\def GET_HIGH_FUSE_BITS
address to read the high fuse bits, using boot_lock_fuse_bits_get
*/
#define GET_HIGH_FUSE_BITS (0x0003)
/** \ingroup avr_boot
\def boot_lock_fuse_bits_get(address)
Read the lock or fuse bits at \c address.
Parameter \c address can be any of GET_LOW_FUSE_BITS,
GET_LOCK_BITS, GET_EXTENDED_FUSE_BITS, or GET_HIGH_FUSE_BITS.
\note The lock and fuse bits returned are the physical values,
i.e. a bit returned as 0 means the corresponding fuse or lock bit
is programmed.
*/
#define boot_lock_fuse_bits_get(address) \
(__extension__({ \
uint8_t __result; \
__asm__ __volatile__ \
( \
"sts %1, %2\n\t" \
"lpm %0, Z\n\t" \
: "=r" (__result) \
: "i" (_SFR_MEM_ADDR(__SPM_REG)), \
"r" ((uint8_t)(__BOOT_LOCK_BITS_SET)), \
"z" ((uint16_t)(address)) \
); \
__result; \
}))
#ifndef __DOXYGEN__
#define __BOOT_SIGROW_READ (_BV(__SPM_ENABLE) | _BV(SIGRD))
#endif
/** \ingroup avr_boot
\def boot_signature_byte_get(address)
Read the Signature Row byte at \c address. For some MCU types,
this function can also retrieve the factory-stored oscillator
calibration bytes.
Parameter \c address can be 0-0x1f as documented by the datasheet.
\note The values are MCU type dependent.
*/
#define boot_signature_byte_get(addr) \
(__extension__({ \
uint8_t __result; \
__asm__ __volatile__ \
( \
"sts %1, %2\n\t" \
"lpm %0, Z" "\n\t" \
: "=r" (__result) \
: "i" (_SFR_MEM_ADDR(__SPM_REG)), \
"r" ((uint8_t)(__BOOT_SIGROW_READ)), \
"z" ((uint16_t)(addr)) \
); \
__result; \
}))
/** \ingroup avr_boot
\def boot_page_fill(address, data)
Fill the bootloader temporary page buffer for flash
address with data word.
\note The address is a byte address. The data is a word. The AVR
writes data to the buffer a word at a time, but addresses the buffer
per byte! So, increment your address by 2 between calls, and send 2
data bytes in a word format! The LSB of the data is written to the lower
address; the MSB of the data is written to the higher address.*/
/** \ingroup avr_boot
\def boot_page_erase(address)
Erase the flash page that contains address.
\note address is a byte address in flash, not a word address. */
/** \ingroup avr_boot
\def boot_page_write(address)
Write the bootloader temporary page buffer
to flash page that contains address.
\note address is a byte address in flash, not a word address. */
/** \ingroup avr_boot
\def boot_rww_enable()
Enable the Read-While-Write memory section. */
/** \ingroup avr_boot
\def boot_lock_bits_set(lock_bits)
Set the bootloader lock bits.
\param lock_bits A mask of which Boot Loader Lock Bits to set.
\note In this context, a 'set bit' will be written to a zero value.
Note also that only BLBxx bits can be programmed by this command.
For example, to disallow the SPM instruction from writing to the Boot
Loader memory section of flash, you would use this macro as such:
\code
boot_lock_bits_set (_BV (BLB11));
\endcode
\note Like any lock bits, the Boot Loader Lock Bits, once set,
cannot be cleared again except by a chip erase which will in turn
also erase the boot loader itself. */
/* Normal versions of the macros use 16-bit addresses.
Extended versions of the macros use 32-bit addresses.
Alternate versions of the macros use 16-bit addresses and require special
instruction sequences after LPM.
FLASHEND is defined in the ioXXXX.h file.
USHRT_MAX is defined in <limits.h>. */
#if defined(__AVR_ATmega161__) || defined(__AVR_ATmega163__) \
|| defined(__AVR_ATmega323__)
/* Alternate: ATmega161/163/323 and 16 bit address */
#define boot_page_fill(address, data) __boot_page_fill_alternate(address, data)
#define boot_page_erase(address) __boot_page_erase_alternate(address)
#define boot_page_write(address) __boot_page_write_alternate(address)
#define boot_rww_enable() __boot_rww_enable_alternate()
#define boot_lock_bits_set(lock_bits) __boot_lock_bits_set_alternate(lock_bits)
#elif (FLASHEND > USHRT_MAX)
/* Extended: >16 bit address */
#define boot_page_fill(address, data) __boot_page_fill_extended(address, data)
#define boot_page_erase(address) __boot_page_erase_extended(address)
#define boot_page_write(address) __boot_page_write_extended(address)
#define boot_rww_enable() __boot_rww_enable()
#define boot_lock_bits_set(lock_bits) __boot_lock_bits_set(lock_bits)
#else
/* Normal: 16 bit address */
#define boot_page_fill(address, data) __boot_page_fill_normal(address, data)
#define boot_page_erase(address) __boot_page_erase_normal(address)
#define boot_page_write(address) __boot_page_write_normal(address)
#define boot_rww_enable() __boot_rww_enable()
#define boot_lock_bits_set(lock_bits) __boot_lock_bits_set(lock_bits)
#endif
/** \ingroup avr_boot
Same as boot_page_fill() except it waits for eeprom and spm operations to
complete before filling the page. */
#define boot_page_fill_safe(address, data) \
do { \
boot_spm_busy_wait(); \
eeprom_busy_wait(); \
boot_page_fill(address, data); \
} while (0)
/** \ingroup avr_boot
Same as boot_page_erase() except it waits for eeprom and spm operations to
complete before erasing the page. */
#define boot_page_erase_safe(address) \
do { \
boot_spm_busy_wait(); \
eeprom_busy_wait(); \
boot_page_erase (address); \
} while (0)
/** \ingroup avr_boot
Same as boot_page_write() except it waits for eeprom and spm operations to
complete before writing the page. */
#define boot_page_write_safe(address) \
do { \
boot_spm_busy_wait(); \
eeprom_busy_wait(); \
boot_page_write (address); \
} while (0)
/** \ingroup avr_boot
Same as boot_rww_enable() except waits for eeprom and spm operations to
complete before enabling the RWW mameory. */
#define boot_rww_enable_safe() \
do { \
boot_spm_busy_wait(); \
eeprom_busy_wait(); \
boot_rww_enable(); \
} while (0)
/** \ingroup avr_boot
Same as boot_lock_bits_set() except waits for eeprom and spm operations to
complete before setting the lock bits. */
#define boot_lock_bits_set_safe(lock_bits) \
do { \
boot_spm_busy_wait(); \
eeprom_busy_wait(); \
boot_lock_bits_set (lock_bits); \
} while (0)
#endif /* _AVR_BOOT_H_ */