26 SAM True Random Number Generator (TRNG) Driver
This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's True Random Number Generator functionality.
The following driver API modes are covered by this manual:
Polled APIs
Callback APIs
The following peripheral is used by this module:
TRNG (True Random Number Generator)
The following devices can use this module:
Atmel | SMART SAM L21/L22
The outline of this documentation is as follows: