6 SAM Digital-to-Analog (DAC) Driver
This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the conversion of digital values to analog voltage. The following driver API modes are covered by this manual:
Polled APIs
Callback APIs
The following peripheral is used by this module:
DAC (Digital-to-Analog Converter)
The following devices can use this module:
Atmel | SMART SAM L21
The outline of this documentation is as follows: