41.8.3 Control B Set

The user can change this register without doing a read-modify-write operation. Changes in this register will, also, be reflected in the Control B Clear (CTRLBCLR) register.
Name: CTRLBSET
Offset: 0x05
Reset: 0x00
Property: PAC Write-Protection, Write-Synchronized, Read-Synchronized

Bit 76543210 
 CMD[2:0]IDXCMD[1:0]ONESHOTLUPDDIR 
Access R/WR/WR/WR/WR/WR/WR/WR/W 
Reset 00000000 

Bits 7:5 – CMD[2:0] TCC Command

These bits can be used for software control of the re-triggering and stop commands of the TCC. When a command is executed, the CMD bit field will be read back as zero. The commands are executed on the next prescaled GCLK_TCCx clock cycle.

Writing a ‘0’ to this bit has no effect.

Writing a valid value to this bit group, as shown in the following table, will set the associated command.
Important: This command requires synchronization before executing it. The following is a valid sequence:
  • Issue CMD command (CTRLBSET.CMD = command)
  • Wait for CMD synchronization (SYNCBUSY.CTRLB = 0)
  • Wait for CMD read back as zero (CTRLBSET.CMD = 0)
ValueNameDescription
0x0NONENo action
0x1RETRIGGERForce start, restart or retrigger
0x2STOPForce stop
0x3UPDATEForce update of double buffered registers
0x4READSYNCForce a read synchronization of COUNT
0x5DMAOSOne-shot DMA trigger

Bits 4:3 – IDXCMD[1:0] Ramp Index Command

These bits can be used to force cycle A and cycle B changes in the RAMP2 and RAMP2A operation. On the timer/counter update condition, the command is executed, the IDX flag in the STATUS register is updated and the IDXCMD command is cleared.

Writing a ‘0’ to this bit has no effect.

Writing a valid value to these bits will set a command.

ValueNameDescription
0x0DISABLECommand disabled: IDX toggles between cycles A and B
0x1SETSet IDX: cycle B will be forced in the next cycle
0x2CLEARClear IDX: cycle A will be forced in next cycle
0x3HOLDHold IDX: the next cycle will be the same as the current cycle.

Bit 2 – ONESHOT One-Shot

This bit controls one-shot operation of the TCC. When in one-shot operation, the TCC will stop counting on the next overflow/underflow condition or a stop command.

Writing a ‘0’ to this bit has no effect.

Writing a ‘1’ to this bit will enable the one-shot operation.

ValueDescription
0The TCC will count continuously.
1The TCC will stop counting on the next underflow/overflow condition.

Bit 1 – LUPD Lock Update

This bit controls the update operation of the TCC buffered registers.

When CTRLB.LUPD is set, the hardware UPDATE registers, with the value from their buffered registers, are disabled. Disabling the update ensures that all buffer registers are valid before a hardware update is performed. After all the buffer registers are loaded correctly, the buffered registers can be unlocked.

This bit has no effect when the input capture operation is enabled.

Writing a ‘0’ to this bit has no effect.

Writing a ‘1’ to this bit will disable the register's updates on the hardware UPDATE condition.

ValueDescription
0The CCBx, PERB, PGVB and PGEB buffer registers values are copied into the corresponding CCx, PER, PGV and PGE registers on hardware update condition.
1The CCBx, PERB, PGVB and PGEB buffer registers values are not copied into CCx, PER, PGV and PGE registers on hardware update condition.

Bit 0 – DIR Counter Direction

This bit is used to change the direction of the counter.

Writing a ‘0’ to this bit has no effect.

Writing a ‘1’ to this bit will set the bit and make the counter count down.
Note: When TCC is counting down, ensure to initialize the COUNT register to the TOP value (PER or CC0 value, depending on the mode).
ValueDescription
0The timer/counter is counting up (incrementing).
1The timer/counter is counting down (decrementing).