3.4 USB Connectivity using Microchip USB 2.0 Hub Controller
The WBZ451HPE Curiosity Board has two USB end device PKOB4 and MCP2200.
Both these USB devices are accessible to the upstream PC via a common USB connector
using Microchip USB 2.0 High Speed Hub Controller USB2512B providing the user with more
ease of use.Figure 3-4. USB Connectivity using Hub
Controller
When the WBZ451HPE Curiosity Board is plugged into the upstream PC using
a USB Type-C cable, the device enumeration is as shown in the
following figure for the PKOB4 and MCP2200. Figure 3-5. Device Manager