6.1 Setting Up the Bluetooth Nodes
The following are the steps to set up a wireless Bluetooth node:
- Connect the RN4678 PICtail board’s PICtail Header J1 to the PIC18 Explorer Development board’s J3 connector.
- The following figure illustrates the position of
jumpers and switches on the PIC18 Explorer board. Set the jumpers/positions on the
PIC18 Explorer Development board as follows:
- Remove the JP3 and connect J7 Pin No 10 (RH0) to JP3 top side pin
- JP1 to enable LEDs
- J13 to ensure that communication is routed through the RS-232 socket
- J4 to ensure the Main PIC is programmed
- Switch S4 to enable Processor In Module (PIM) (pointing towards MPLAB REAL ICE In-Circuit Emulator when ON).
- Use the switches (S1 and S2) and LCD (LCD1) on the PIC18 Explorer Development board for configuring and monitoring the wireless terminals.
- Connect the programmer or debugger (MPLAB REAL ICE In-Circuit Emulator, MPLAB ICD 3 or PICkit 3) to the PIC18 Explorer Development board.
- Plug-in the 9V power supply to the PIC18 Explorer Development board through the 9V adapter (wall power) or through a 9V battery, as illustrated in the following figure.
- Open the downloaded application demo source code and compile it. Alternatively, in
the download folder, use the precompiled
RN4678_MCU18_Interface.X.production.hexfile. - The generated or precompiled
RN4678_MCU18_Interface.X.production.hexfile can, then, be programmed into the two wireless nodes A and B using any of the Microchip devices supporting the PIC18F87J11. - The boards are now ready to run the
demo. In some instances, it is necessary to run a Hardware Reset to run the code,
specifically in the case of the PIC18 Explorer Development board.Note:
- Only connect the 9V battery supply to the PIC18 board if a battery socket provision is made, as illustrated in the following figure.
- For the application demo, use the 9VMN1604 (9V-6LF22, alkaline manganese dioxide) battery.
For additional information on programming/debugging with the MPLAB ICD 3, refer to the MPLAB® ICD 3 In-Circuit Debugger User's Guide for MPLAB X IDE. For more details on the PIC18 Explorer Development board, refer to the PICDEM™ PIC18 Explorer Demonstration Board User's Guide.