4.2.3 Wi-Fi Hotspot (AP) Mode
In AP mode, the WINC allows Wi-Fi stations to connect and obtain the IP
address from the WINC DHCP server. To enter AP mode, the host MCU application calls
m2m_wifi_enable_ap API. To exit AP mode, the application calls
m2m_wifi_disable_ap API.
The supported API functions in this mode use the HIF command types:
tenuM2mApCmd and tenuM2mConfigCmd. See the full
list of commands in the m2m_types.h header file.
For more information about this mode, refer to Wi-Fi AP Mode.