4.2.2 Wi-Fi Station Mode
The ATWINC15x0 enters Station (STA) mode when
the host MCU requests connection to an AP using the
m2m_wifi_connect or
m2m_wifi_default_connect APIs. The ATWINC15x0
exits STA mode when it receives a disconnect request from the Wi-Fi AP conveyed to the
host MCU application via the event callback
M2M_WIFI_RESP_CON_STATE_CHANGED or when the host MCU application
decides to terminate the connection via m2m_wifi_disconnect API.Note: The supported API functions in this
mode use the HIF command types:
tenuM2mConfigCmd and
tenuM2mStaCmd. See the full list of commands in the
m2m_types.h header file.For more information about STA mode, refer to Wi-Fi Station Mode.