3.4.2 Interrupt Handling
The HIF interrupts the host MCU when one or more events are pending in the
ATWINC15x0 firmware. The host MCU application is a big
state machine which processes received data and events when the ATWINC15x0 driver calls the event callback function(s). To receive event
callbacks, the host MCU application is required to call the
m2m_wifi_handle_events API to let the host driver retrieve and
process the pending events from the ATWINC15x0 firmware. It
is recommended to call this function if any of the following events occur:
- The host MCU application polls the API in main loop or a dedicated task
- When the host MCU receives an interrupt from the ATWINC15x0 firmware
m2m_wifi_handle_events API.- Host MCU with no operating system configuration – the MCU main loop is responsible to handle deferred work from the interrupt handler
- Host MCU with operating system
configuration – a dedicated task or thread is required to call
m2m_wifi_handle_eventsto handle deferred work from the interrupt handler
- Host driver entry point
m2m_wifi_handle_eventsis non-reentrant. In the operating system configuration, it is required to protect the host driver from reentrance by a synchronization object. - When the host MCU is polling
m2m_wifi_handle_events, the API checks for pending unhandled interrupt from the ATWINC15x0. If no interrupt is pending, it returns immediately. If an interrupt is pending,m2m_wifi_handle_eventssequentially reads all the pending HIF messages and dispatches the HIF message content to the respective registered callback. If a callback is not registered to handle the type of message, the HIF message content is discarded.