1.34.27.40 USARTx_SPI_CallbackRegister Function
C
/* x = USART SPI instance number */
/* USART SPI master (non-blocking mode) mode */
void USARTx_SPI_CallbackRegister(USART_SPI_CALLBACK callback, uintptr_t context )
Summary
This function allows application to register a callback function for the PLIB to call back when the requested data transfer operation has completed.
Description
This function sets the pointer to a client/application function to be called "back" when the given USARTx_SPI's transfer events occur. It also passes a context value (usually a pointer to a context structure) that is passed into the function when it is called. The specified callback function will be called from the peripheral interrupt context. The callback should be registered before a transfer operation is requested.
Precondition
The USARTx_SPI_Initialize function must have been called. This function is only available if the library is configured for interrupt operation mode.
Parameters
Param | Description |
---|---|
callback | A pointer to a function with a calling signature defined by the USART_SPI_CALLBACK data type. Setting this to NULL disables the callback feature. |
context | A value (usually a pointer) which is passed (unused) into the function identified by the callback parameter |
Returns
None.
Example
-
USART SPI master (non-blocking mode) mode*
uint8_t txBuffer[4]; uint8_t rxBuffer[10]; size_t txSize = 4; size_t rxSize = 10; bool reqAccepted; void APP_USART1_SPITransferHandler(uintptr_t context) { //Transfer was completed without error, do something else now. } USART1_SPI_Initialize(); USART1_SPI_CallbackRegister(&APP_USART1_SPITransferHandler, (uintptr_t)NULL); if(USART1_SPI_WriteRead(&txBuffer, txSize, &rxBuffer, rxSize)) { // request got accepted } else { // request didn't get accepted, try again later with correct arguments }
Remarks
None