1.34.27.22 USARTx_ReadAbort Function
C
/* x = USART instance number */
/* Non-blocking mode */
bool USARTx_ReadAbort(void)
Summary
Aborts the ongoing read request
Description
This API lets the application abort an ongoing read request. If needed, the application can call the USARTx_ReadCountGet API to know the number of bytes successfully read before issuing the USARTx_ReadAbort API.
Precondition
USARTx_Initialize must have been called for the associated USART instance and a read request is already submitted.
Parameters
None
Returns
true - operation is successful
false - error during execution
Example
bool timeout; if (timeout == true) { // Kill the ongoing read read request USART1_ReadAbort(); }
Remarks
None