1.28.2.5 ADC_ChannelsInterruptDisable Function
C
void ADC_ChannelsInterruptDisable(ADC_INTERRUPT_MASK channelsInterruptMask) void ADC_ChannelsInterruptDisable(ADC_INTERRUPT_EOC_MASK channelsInterruptMask)
Summary
Disables the ADC interrupt sources
Description
This function disables interrupt sources specified in channelsInterruptMask.
Precondition
ADC_Initialize() function must have been called first for the associated instance.
Parameters
Param | Description |
---|---|
channelsInterruptMask | interrupt sources |
Returns
None.
Example
ADC_Initialize();
ADC_ChannelsInterruptDisable(ADC_INTERRUPT_EOC_0_MASK);
Remarks
This function does not disable interrupts which are not included in the mask.