1.28.2.3 ADC_ChannelsDisable Function
C
void ADC_ChannelsDisable (ADC_CHANNEL_MASK channelsMask)
Summary
Disables the ADC channels
Description
This function disables channels specified in channelsMask
Precondition
ADC_Initialize() must have been called first for the associated instance.
Parameters
Param | Description |
---|---|
channelsMask | set of channel numbers |
Returns
None.
Example
ADC_Initialize(); ADC_ChannelsDisable(ADC_CH0_MASK | ADC_CH3_MASK);
Remarks
This function does not enable channels which are not included in the channel mask.