1.30.17.7 TCCx_Timer24bitCompareSet Function

C

void TCCx_Timer24bitCompareSet ( uint32_t compare );

Summary

Sets the compare value of a given timer channel.

Description

This function writes the compare value. When timer counter matches compare value, interrupt can be generated.

Precondition

TCCx_TimerInitialize function must have been called first for the given channel.

Parameters

Param Description
compare compare value of the timer

Returns

None.

Example

TCC0_TimerInitialize();
TCC0_Timer24bitCompareSet(0xFul);

Remarks

This function is available only when TCC timer mode is used by SYS_TIME module. SYS_TIME uses compare match interrupt to generate dynamic delay.