1.28.22.19 SDMMCx_BlockSizeSet Function

C

/* x = SDMMC instance number */

void SDMMCx_BlockSizeSet ( uint16_t blockSize )

Summary

Sets the size of the one data block of transfer.

Description

Sets the size of the one data block of transfer.

Precondition

SDMMCx_Initialize() must have been called first for the associated instance.

Parameters

Param Description
blockSize Size of one block of transfer

Returns

None.

Example

SDMMC1_BlockSizeSet(512);

Remarks

None.