1.25.3.19 CANx_RxCallbackRegister Function
C
bool CANx_RxCallbackRegister(CAN_CALLBACK callback, uintptr_t contextHandle, CAN_MAILBOX_RX_ATTRIBUTE mailboxAttr) // x - Instance of the CAN peripheral
Summary
Sets the pointer to the function (and it's context) to be called when the given CAN's Rx transfer events occur.
Precondition
CANx_Initialize must have been called for the associated CAN instance.
Parameters
Param | Description |
---|---|
callback | A pointer to a function with a calling signature definedby the CAN_CALLBACK data type. |
contextHandle | A value (usually a pointer) passed (unused) into the functionidentified by the callback parameter. |
mailboxAttr | Mailbox type either RX Mailbox or RX Mailbox with overwrite |
Returns
Request status. true - Request was successful.
false - Request has failed.
Example
void CAN0_callbackHandler (uintptr_t context)
{
}
CAN0_RxCallbackRegister(CAN0_callbackHandler, 0, CAN_MAILBOX_DATA_FRAME_RX_OVERWRITE);
CAN0_MessageReceive(&rx_messageID, &rx_messageLength, rx_message, ×tamp, CAN_MAILBOX_DATA_FRAME_RX_OVERWRITE);
Remarks
None.