2.58.13 INTC_Restore Function
C
void INTC_Restore( bool state )
Summary
Restores the state of global interrupts before the disable occurred.
Description
This function restores the state of global interrupts to the specified state that was saved prior to the disable operation. This is typically used to re-enable interrupts after they were temporarily disabled.
Precondition
The state must be previously saved using the INTC_Disable() function.
Parameters
state - The interrupt status to restore, typically obtained from the INTC_Disable() function.
Returns
None.
Example
bool prevStatus = INTC_Disable(); INTC_SourceEnable(INT_SOURCE_INT0); INTC_Restore(prevStatus);
Remarks
None.