2.58.5 INTC_SourceDisable Function
C
void INTC_SourceDisable( INT_SOURCE source );
Summary
Disables the interrupt source.
Description
This function disables the given interrupt source.
This API performs a Read-Modify-Write (RMW) operation on the IECx register. To prevent race conditions, please disable global interrupts using `INTC_Disable` API before calling this function.
Precondition
INTC_Initialize() function must have been called first.
Parameters
| Param | Description |
|---|---|
| source | One of the possible values from INT_SOURCE. |
Returns
None.
Example
bool prevStatus = INTC_Disable(); INTC_SourceDisable(INT_SOURCE_INT0); INTC_Restore(prevStatus);
Remarks
This function implements an operation of the SourceControl feature. This feature may not be available on all devices. Please refer to the specific device data sheet to determine availability.