2.52.7 HEFC_RegionLock Function
C
void HEFC_RegionLock(uint32_t address);
Summary
Locks a Flash region.
Description
This function is used to lock a certain region of on-chip flash. It takes in address as a parameter and locks the region associated with it.
Precondition
Validate if HEFC controller is ready to accept new request by calling HEFC_IsBusy()
Parameters
| Param | Description |
|---|---|
| address | Address of the page to be locked |
Returns
None.
Example
HEFC_RegionLock(0x10010000);
while(HEFC_IsBusy());