2.42.6 EIC_FreezeConfiguration Function
C
bool EIC_FreezeConfiguration(EIC_PIN pin)
Summary
Freeze EIC configuration.
Description
Calling this API freezes the configurations of an EIC pin. Any further API calls changing the behavior of the EIC will return false.
Precondition
EIC_Initialize() must have been called first for the associated instance.
Parameters
Param | Description |
---|---|
pin | EIC Pin number |
Returns
bool - Status of the API call.
Example
EIC_FreezeConfiguration(EIC_PIN_0);
Remarks
None.