4.3.2 Connections and Protocols

Click a tab to the left of the window to see available connections and protocols. After you connect a target to the PC, that connection will be displayed in the Connections tab and the on-board data sources will be listed. Some sources have options that can be set using the Source options button . Select to plot the raw source data. If you are connected and wish to change the settings, you can disconnect by clicking . Make your changes and then click the button again to reconnect.

Sources that are not a part of a group can also be plotted on the Time Plot by dragging and dropping. Drop on an axis to add the source to it, or on a plot to add it to the rightmost axis on that plot. Holding shift while dropping on axis or plot adds the source on a new axis on the same plot. You can also place the source on a new axis on a new plot above or below by dropping on the upper or lower area of the plot.