4.8.2.3.2 Write Variables

The Write Variables widget is a button that writes values to variables defined on a protocol session. It can only be used with a protocol session that supports loading an ELF file, which must be loaded before configuring the widget.

Selecting Variables

See Read Variables

Writing Variables

For output widgets added to the dashboard, variables selected as described above will appear in the source selection list. Once other widgets are connected, make sure those widgets send a value (e.g. by editing their value). Then, pressing the button will write the values to the target.

Configuration

See Read Variables