4.8.2.1.3 Table

The Table widget displays one or more data sources in a table. Two modes are supported: Manual Labels and Auto Labels. In Manual Labels mode each cell can be manually configured to either be a Label cell or a Data cell. In Auto Labels mode, each cell is split into two fields, where the field to the left is a label with the name of the data stream and the field to the right is the actual data of the stream. The mode is selected by the check box named Auto Labels in the configuration.

Manual Labels

When using Manual Labels mode each cell either is a Label cell or a Data cell. By default all cells are Data cells. Label cells can be configured by setting the Label value (see figure below).

Only the Data cells have data fields.

Auto Labels

Each cell is associated with one data source and the name of the data source is shown to the left in the cell and the actual data to the right. The source name is automatically fetched from the source connected to the sink data field.

The Table element has one data field per table cell accepting any data source. The data will be converted to a string and displayed as text.

Resize Table

Cell sizes are treated as a minimum size. If the table is resized to be larger than the sum of cell sizes, the cells grow proportionally. If the table is shrunk to be smaller than the sum of cell sizes, the table will maintain a minimum size and overflow the widget, as shown below.

It is possible to have the table widget dynamically resized by clearing the width and height values (clicking on the 'x' button for those values).

Figure 4-64. Table after resize - overflow

Configuration

Hover over parameters in visualizer for more information.

Table 4-19. Dimensions Group
ParameterTypeUsage
Row CountNumericNumber of rows in the table
Col. CountNumericNumber of columns in the table
Auto LabelsCheck boxCheck to use Auto Labels
Table 4-20. Colors Group
Parameter Type Usage
Foreground Color selection dialog Color of widget foreground.
Background Color selection dialog Color of widget background.
Table 4-21. Label Cells, Data Cells Group
ParameterTypeUsage
Min. WidthNumericWidth of the label or data part of each cell. Note that changing this width will change the total width of the table.
Min. HeightNumericHeight of the label or data part of each cell. Note that changing this height will change the total height of the table.
Font SizeNumericEnter font size.
Font WeightDrop down boxSelect from Normal or Bold.
Font StyleDrop down boxSelect from Normal or Italics.
Font FamilyDrop down boxSelect Segment.
HorizontalDrop down boxSelect the horizontal alignment of cell contents.