13.4 Functional Description
PIC32CM LE00 Boot ROM
First the PIC32CM LE00 Boot ROM checks if a debugger is present to enter the Boot Interactive mode which allows the user to perform specific tasks through a debugger connection.
PIC32CM LS00/LS60 Boot ROM
The PIC32CM LS00/LS60 Boot ROM sequence consists in performing several security tasks (integrity checks, memories and peripherals security attribution, Secure Boot, DICE CDI key generation...) before starting the application.
The Boot ROM first checks if a debugger is present to enter the Boot Interactive mode which allows the user to perform specific tasks via a debugger connection.
Device Integrity Checks
- The User Row CRC
(USERCRC) which is located in the NVM User Row (UROW) at:
UROW Offset Bit Position Name 0x20-0x23 287:256 USERCRC - The Boot Configuration
Row CRC (BOCORCRC) which is located in the NVM Boot Configuration Row
(BOCOR) at:
BCOR Offset Bit Position Name 0x08-0x0B 95:64 BOCORCRC
User Row CRC (USER CRC)
USERCRC allows to check the following fuses parameters integrity:
- AS, ANSC, DS, RS
- URWEN
- NONSECA, NONSECB, NONSECC
- CDIROFFSET
USERCRC is the CRC of the NVM User row area which starts from 0x00804008 and finish at 0x0080401F (bit 64 to bit 255):
Offset | Bit Pos. | Name | |||||||
---|---|---|---|---|---|---|---|---|---|
0x08 | 71:64 | AS | |||||||
0x09 | 79:72 | ANSC | AS | ||||||
0x0A | 87:80 | DS | Reserved | ANSC | |||||
0x0B | 95:88 | Reserved | DS | ||||||
0x0C | 103:96 | RS | |||||||
0x0D | 111:104 | Reserved | URWEN | Reserved | RS | ||||
0x0E-0xF | 127:112 | Reserved | |||||||
0x10-0x13 | 159:128 | NONSECA | |||||||
0x14-0x17 | 191:160 | NONSECB | |||||||
0x18-0x1B | 223:192 | NONSECC | |||||||
0x1C-0x1F | 255:224 | CDIROFFSET |
Boot Configuration Row CRC (BOCORCRC)
BOCORCRC allows to check the following fuses parameters integrity:
- BOOTPROT, BNSC, BOOTOPT
- SECCFGLOCK, DICEEN
- BCWEN, BCREN
BOCORCRC is the CRC of the NVM Boot Configuration row area, which starts from 0x0080C000 and finish at 0x00800C007 (bit 0 to bit 63).
Offset | Bit Pos. | Name | |||||||
---|---|---|---|---|---|---|---|---|---|
0x00-0x1 | 15:0 | Reserved | |||||||
0x02 | 23:16 | BNSC | Reserved | ||||||
0x03 | 31:24 | Reserved | BNSC | ||||||
0x04 | 39:32 | BOOTOPT | |||||||
0x05 | 47:40 | BOOTPROT | |||||||
0x06 | 55:48 | Reserved | DICEEN | SECCFGLOCK | BOOTPROT | ||||
0x07 | 63:56 | Reserved | BCREN | BCWEN |
- This will allow, if a debugger is connected, to put the device in the highest debug access level mode (DAL = 2) by issuing a Chip Erase command . Once in that mode, it is possible for a programming tool to reprogram the NVM Configuration Rows.
- When the check fails and no debugger is connected, the part will reset and restart the check sequence again.
CRC Computation and Programming
The CRCs needs to be recalculated and updated in their respective NVM Configuration row as soon as a data from any of the checked regions is changed.
- Width = 32 bits
- Polynomial = 0x04C11DB7 (Poly)
- Initial Value = 0xFFFFFFFF (Init)
- Input Data is reflected (RefIn)
- Output Data is reflected (RefOut)
- No XOR is performed on the output CRC (XorOut)
Example: the DSU CRC of 0x31, 0x32, 0x33, 0x34, 0x35, 0x36, 0x37, 0x38, 0x39 is 0x340BC6D9
Memories and Peripherals Configurations Initialization
For PIC32CM LS00/LS60 devices, memories and peripherals security attributions are done by reading the different fuses values from the NVM User (UROW) and Boot Configuration (BOCOR) rows.
- Set memory security attribution according to AS, ANSC, DS, RS, BNSC and BOOTPROT fuses
- Set peripherals security attribution according to NONSECA, NONSECB and NONSECC fuses
Secure Boot
- The BOOTPROT region which
is composed by:
- The Secure Flash (BOOT region)
- The Non-Secure Callable Flash (BOOT region)
- The NVM Boot Configuration row (BOCOR)
BOOTOPT | BOOTPROT region Verification Method | NVM Boot Configuration Row (BOCOR) |
---|---|---|
0 | Secure Boot Disabled | |
1 | SHA-256 | |
2 | SHA-256 with BOOTKEY(1) | |
3 | HMAC with BOOTKEY(1) | |
Others | Reserved |
- BOOTKEY is defined in BOCOR row
BOOTOPT | BOOTPROT region Verification Method | NVM Boot Configuration Row (BOCOR) |
---|---|---|
0 | Secure Boot Disabled | |
1 | SHA-based Secure Boot | |
2 | SHA-based Secure Boot with BOOTKEY(1) | |
3 | HMAC-based Secure Boot with BOOTKEY(1) | |
4 | ATECC608B-based Secure Boot | SHA |
5 | ATECC608B-based Secure Boot | SHA with BOOTKEY(1) |
6-255 | ATECC608B-based Secure Boot | HMAC with BOOTKEY(1) |
- BOOTKEY is defined in BOCOR row
If the verification fails, the Boot ROM will report the error to the DSU peripheral and will enter the Boot Interactive mode. This will allow, if a debugger is connected, to put the device in the highest debug level access mode (DAL = 2) by issuing a Chip Erase command. Once in that mode, it is possible for a programming tool to reprogram the different memory regions and/or NVM Configuration rows.
When verification fails and no debugger is connected, the part will reset and restart the integrity checks sequences again.
BOOTPROT Region Verification Using SHA-256 or HMAC
The digest (SHA-256) / MAC (HMAC) is computed on the whole BOOTPROT region, which is composed by the Secure Flash (BOOT region) and the Non-Secure Callable Flash (BOOT region).
The digest/MAC reference value for this area is stored at the end of the Secure Flash (BOOT region), just before the Non-Secure Callable Flash (BOOT region).
SHA-256 Verification Method
This verification method uses the standard SHA-256 hash algorithm which produces a digest of 256 bits, i.e. 32 bytes that is compared against the value placed at the end of the Secure Flash (BOOT Region).
SHA-256 with BOOTKEY Verification Method
To prevent unauthorized change of the boot loader code, the digest computation can be slightly modified to require a key to produce a valid digest.
When SHA-256 with BOOTKEY is selected, the digest computation (for both BOOTPROT region and NVM BOCOR row) starts by processing the secure boot key (BOOTKEY) data twice, then proceeds with the rest of data.
BOCOR Offset | Bit Position | Name |
---|---|---|
0x50-0x6F | 895:640 | BOOTKEY |
HMAC with BOOTKEY Verification Method
The verification method uses the standard HMAC hash algorithm (defined in FIPS PUB 198-1).
The hash used for HMAC is SHA-256 which produces a MAC of 256 bits, 32 bytes, that is compared against the value placed at the end of the Secure Flash (BOOT Region). The key used is BOOTKEY from BOCOR NVM Configuration row.
BOOTPROT Region Verification using the ATECC608B (PIC32CM LS60 only)
When BOOTOPT>0, the Boot ROM uses the ATECC608B to assist in authenticating and checking the integrity of an application code (usually a boot loader) that is to be subsequently executed.
This authentication process is done in two steps:
- An ECDSA signature of the application image must first be generated and stored on the application image
- Secure Boot execution will then authenticate the application code
The ECDSA signature (64 bytes) is computed on the overall BOOTPROT region, which is composed by the Secure Flash (BOOT region) and the Non-Secure Callable Flash (BOOT region).
The signature for this area must be stored at the end of the Secure Flash (BOOT region), just before the Non-Secure Callable Flash (BOOT region).
ATECC608B-Based Secure Boot Verification Method
This verification method uses the ATECC608B.
The ATECC608B is configured to operate in the Stored Secure Boot (FullDig) mode, where:
- The digest is stored in Slot 7
- The public key
required to verify the SecureBoot is stored in Slot 15 Note: The public key must be initially provisioned in Slot 15.
The Stored Secure Boot (FullDig) mode executes the ATECC608B SecureBoot command in the following modes:
- FullCopy mode
- FullStore (Digest) mode
FullCopy mode is executed the first time the code used to authenticate is verified: the Boot ROM passes both the digest and signature to the ATECC608B for verification and stores the digest in the ATECC608B.
FullStore (Digest) mode is then executed. In that mode, the Boot ROM passes only the digest to the ATECC608B, which performs a compare with the Digest that has been stored upon the first authentication of the code.
The communication between the PIC32CM LS60 microcontroller and the ATECC608B is encrypted using an I/O Protection Key. This unique key is initially provisioned in both the ATECC608B Slot 6 and the microcontroller BOCOR NVM Configuration Row (IOPROTKEY).
The ATECC608B Slot 6 is not locked by default, hence if a Full ChipErase is done on the microcontroller (where BOCOR IOPROTKEY will be erased), both the microcontroller and the ATECC608B can be provisioned with a new key value.
Refer to the Chapter “I/O Protection Key” from the ATECC608B-TFLXTLS CryptoAuthentication™ Data Sheet to get the ATECC608B commands support this feature.
NVM Boot Configuration Row (BOCOR) Verification
BOCOR Offset | Bit Position | Name |
---|---|---|
0xE0-0xFF | 2047:1792 | BOCORHASH |
Device Identity Composition Engine (DICE)
The Device Identifier Composition Engine (DICE) is a standard developed by the Trusted Computing Group (TCG) for implementing attestation in low cost IoT devices.
BOCOR Offset | Bit Position | Name |
---|---|---|
0x06 | 52 | DICEEN |
UROW Offset | Bit Position | Name |
---|---|---|
0x1C-0x1F | 255:224 | CDIROFFSET |
The Boot ROM checks that CDIROFFSET is within the maximum SRAM range; if not, the CDI is not written.
DICE CDI Key Generation Flow
Unique Device Secret (UDS)
The Unique Device Secret (UDS) is a 256-bit symmetric key used to generate the CDI. The UDS key is only accessible to the DICE engine and is only used for calculating the CDI at boot time.
The Unique Device Secret must be provisioned on BOCOR.UDS fuse. It must be unique for each device and have a strong entropy.
If DICE is enabled but the UDS key is not provisioned (BOCOR.UDS is all 1s), all zeros are written to the CDI output.
Compound Device Identifier (CDI)
The Compound Device Identifier (CDI) is the output of the DICE module that is passed to the boot flash code at a specified memory location in SRAM.
The CDI can be used by the boot flash code directly for attestation or to derive other keys.
The CDI is a 256 bit value calculated as follows:
CDI = HMAC-SHA-256( UDS, H(BOOTPROT region) )
- The hash function H() calculated over the boot Flash image is SHA-256.
- The BOOTPROT region is composed by the Secure Flash (BOOT region) and the NSC Flash (BOOT region)
(or signature)
which is stored in the Secure Flash (BOOT region). This digest/MAC is not included in the computation of the BOOTPROT region for CDI generation, to be independent of the Secure Boot operations.Debug Access Levels
- DAL2: Highest debug level access with no restrictions in term of memory and peripheral accesses.
- DAL0: No access is authorized except with a debugger using the Boot ROM Interactive mode.
The possible transitions between each debug access level are described below:
The PIC32CM LS00/LS60 has the following possible debug access levels (DAL):
- DAL2: Highest debug level access with no restrictions in term of memory and peripheral accesses.
- DAL1: Access is limited to the Non-Secure memory regions. Secure memory regions accesses are forbidden.
- DAL0: No access is authorized except with a debugger using the Boot ROM Interactive mode.
The possible transitions between each debug access level are described below:
For security reasons, increasing the Debug Level Access is only possible during Boot ROM execution and will be always preceded by a specific chip erase depending on the Debug Access Level.
Chip Erase
The Chip erase commands are executed whatever the Flash regions are locked or not. Refer to the Region Unlock Bits in the NVMCTRL chapter.
For PIC32CM LE00, the chip erase command does not require a key.
For PIC32CM LS00/LS60, the chip erase commands are protected with keys (CEKEYx) defined in the NVM BOCOR row.
PIC32CM LS00/LS60 | PIC32CM LE00 | ||||
---|---|---|---|---|---|
Boot ROM Command | ChipErase_NS (CE0) | ChipErase_S (CE1) | ChipErase_ALL (CE2) | ChipErase (CHIPERASE) | ChipErase_ALL (CHIPERASE_ALL) |
Key Requirement | Yes (CEKEY0) | Yes (CEKEY1) | Yes (CEKEY2) | No | |
Flash (BOOT region) | No | Yes | No | Yes | |
Flash (APPLICATION region) | - | Yes | |||
Data Flash | - | Yes | |||
Secure Flash (AS region) | No | Yes | - | ||
Non-Secure Flash (APPLICATION region) | Yes | - | |||
Secure Data Flash (DS) | No | Yes | - | ||
Non-Secure Data Flash | Yes | - | |||
NVM User Row (UROW) | No | Yes | No | Yes | |
NVM Boot Configuration Row (BOCOR) | No | Yes | No | Yes | |
Volatile Memories | Yes | Yes | |||
Debugger Access Level after reset | 2 (if DAL was 2) else 1 | 2 (if DAL was 2 or BOOTPROT==0) else 1 | 2 | 2 |
Boot ROM Interactive Mode
The interactive mode allows the user to perform several actions on the device during the Boot ROM execution through a debugger connection.
Enter Interactive Mode (CMD_INIT)
This command allows launching the Boot Interactive command mode of the Boot ROM.
When CRSTEXT is cleared, CPU starts Boot ROM Interactive mode execution. After a small delay (5 ms is advised), the debugger must check if the Boot ROM has not flagged any errors by checking the BCCD1 bit in the DSU.STATUSB register.
If errors are reported, the debugger can get the error type by checking the DSU.BCC1 register from the DSU external address space.
If no error is reported, the debugger writes the CMD_INIT command to the DSU.BCC0 register to request Boot ROM Interactive mode entry. When command is successful, Boot ROM will place the “SIG_COMM” status in the DSU.BCC1 register.
CMD_INIT
Exit Interactive Mode (CMD_EXIT)
This command allows exiting the Boot Interactive mode.
- The application
- The CPU Park mode
CMD_EXIT
System Reset Request (CMD_RESET)
This command allows resetting the system using a system reset request, because the reset is executed immediately after receiving the command, no reply is sent to the debugger.
After reset, the CPU executes the Boot ROM code from the beginning.
PIC32CM LE00 Chip Erase (CMD_CHIPERASE and CMD_CHIPERASE_ALL)
The CMD_CHIPERASE command erases the entire device except BOOT area, and reverts to Debug Access Level 2.
The CMD_CHIPERASE_ALL command erases the entire device including the BOOT area, and reverts to Debug Access Level 2.
PIC32CM LS00/LS60 Chip Erase (CMD_CEx)
The CMD_CEx commands are used to erase specific part of the device and to increase the Debug Access Level.
NVM Memory Regions Integrity Checks (CMD_CRC)
The Boot ROM provides a way to check the integrity of the embedded non-volatile memories which may be of interest in case of a failure analysis.
This requires the user to place tables describing the memory area to be checked with their expected CRC values.
CRC Table format
Description | Header | Start Address (1) | Size in bytes (2) | Expected value (3) |
---|---|---|---|---|
Field | HDR | ADDR | SIZE | REFVAL |
Offset | 0x0 | 0x4 | 0x8 | 0xC |
Value | 0x43524349 | 0x00000000 | 0x100 | 0xAABBCCDD |
Note 1: ADDR must be a multiple of 4 (only ADDR[31:2] are used).
Note 2: SIZE must be a multiple of 4 (only SIZE[31:2] are used).
Note 3: The expected value is the computed CRC32 value of the memory target.
Requirements
- Each table occupies 16 bytes in memory.
- The table must start at a 16 byte aligned address. (i.e. 0xXXXXXXX0)
- The table must be
placed in the same memory region as its target memory range. (i.e. a
table placed in the Secure Flash (APPLICATION region) can only
target Secure Flash (APPLICATION region) memory addresses).The exceptions to this rule are as follows:
- For PIC32CM LE00: all non-volatile memories are considered as a single region (e.g. a table located in Data Flash can target Flash)
- For PIC32CM LS00/LS60: ANSC and BNSC regions are considered to belong to the same region as their “parent” region: AS for ANSC and BOOTPROT for BNSC.
CRC Command Key
BOCOR Offeset | Bit Position | Name |
---|---|---|
0x40-0x4F | 639:512 | CRCKEY |
Similar to the ChipErase keys, the key can be set to all ‘0s’ to prevent any access to the command.
CMD_CRC
Random Session Key Generation (CMD_DCEK) - PIC32CM LS00/LS60 only
This command allows using a challenge-response scheme to prevent exposure of the keys in clear text on the debugger communication lines.
The different keys sent by the debugger during the Boot ROM for Chip Erase (CMD_CEx) and CRC (CMD_CRC) commands execution are:
- CRCKEY for CMD_CRC command
- CEKEYx for CMD_CEx commands
The random challenge value is generated using the TRNG of the device. It is generated once the CMD_DCEK is received and communicated to the debugger.
The next CMD_CEx or CMD_CRC commands will expect the key value to be replaced by the computed response corresponding to the challenge.
The challenge value is valid only for the next CMD_CEx/ CMD_CRC command.
Before sending a new CMD_CEx/ CMD_CRC command, a CMD_DCEK shall be used to re-enable the challenge-response scheme a get a new challenge value.
On the debugger side, the response shall be computed using the following algorithm:

Where KeyIndex is:
- 0 for ChipErase_NS
- 1 for ChipErase_S
- 2 for ChipErase_ALL
- 3 for CRC Command
- HMAC is described in FIPS PUB 198-1.
- The hash used for HMAC is SHA-256.
- The output of the HMAC-SHA-256 is truncated to obtain an HMAC-SHA-256-128 as explained in RFC4868.
CMD_DCEK (PIC32CM LS00/LS60 only)
NVM Configuration Rows Content Checks (CMD_RAUX)
The Boot ROM provides a way to check the content of the NVM Configuration rows.
When device is secured (DAL0), the fuse configuration can still be read by the debugger using the Read Auxiliary command (CMD_RAUX).
Area | Start address | End address |
---|---|---|
User row (UROW) | 0x00804000 | 0x008040FF |
Software Calibration row | 0x00806020 | 0x00806023 |
- Boot Configuration row (BOCOR) is not accessible by the Read Auxiliary Row command.
CMD_RAUX
Note: After the CMD_RAUX is sent, the debugger can read multiple data, the read loop is exit when an out of range address is sent.
Boot Interactive Mode Commands
Command Name | Description | Command prefix | Command |
---|---|---|---|
CMD_INIT | Entering Interactive Mode | 0x444247 | 55 |
CMD_EXIT | Exit Interactive Mode | 0x444247 | AA |
CMD_RESET | System Reset Request | 0x444247 | 52 |
CMD_CE0 | ChipErase_NS for PIC32CM LS00/LS60 | 0x444247 | E0 |
CMD_CE1 | ChipErase_S for PIC32CM LS00/LS60 | 0x444247 | E1 |
CMD_CE2 | ChipErase_ALL for PIC32CM LS00/LS60 | 0x444247 | E2 |
CMD_CHIPERASE | ChipErase for PIC32CM LE00 | 0x444247 | E3 |
CMD_CHIPERASE_ALL | ChipErase_ALL for PIC32CM LE00 | 0x444247 | E4 |
CMD_CRC | NVM Memory Regions Integrity Checks | 0x444247 | C0 |
CMD_DCEK | Random Session Key Generation for PIC32CM LS00/LS60 | 0x444247 | 44 |
CMD_RAUX | NVM Configuration Rows Integrity Checks | 0x444247 | 4C |
Boot Interactive Mode Status
Status Name | Description | Status prefix | Status coding |
---|---|---|---|
SIG_NO | No Error | 0xEC0000 | 00 |
SIG_SAN_FFF | Fresh from factory error | 0xEC0000 | 10 |
SIG_SAN_UROW | UROW checksum error | 0xEC0000 | 11 |
SIG_SAN_SECEN | SECEN parameter error | 0xEC0000 | 12 |
SIG_SAN_BOCOR | BOCOR checksum error | 0xEC0000 | 13 |
SIG_SAN_BOOTPROT | BOOTPROT parameter error | 0xEC0000 | 14 |
SIG_SAN_NOSECREG | No secure register parameter error | 0xEC0000 | 15 |
SIG_COMM | Debugger start communication command | 0xEC0000 | 20 |
SIG_CMD_SUCCESS | Debugger command success | 0xEC0000 | 21 |
SIG_CMD_FAIL | Debugger command fail | 0xEC0000 | 22 |
SIG_CMD_BADKEY | Debugger bad key | 0xEC0000 | 23 |
SIG_CMD_VALID | Valid command | 0xEC0000 | 24 |
SIG_CMD_INVALID | Invalid command | 0xEC0000 | 25 |
SIG_ARG_VALID | Valid argument | 0xEC0000 | 26 |
SIG_ARG_INVALID | Invalid argument | 0xEC0000 | 27 |
SIG_CE_CVM | Chip erase error: CVM | 0xEC0000 | 30 |
SIG_CE_ARRAY_ERASEFAIL | Chip erase error: array erase fail | 0xEC0000 | 31 |
SIG_CE_ARRAY_NVME | Chip erase error: array NVME | 0xEC0000 | 32 |
SIG_CE_DATA_ERASEFAIL | Chip erase error: data erase fail | 0xEC0000 | 33 |
SIG_CE_DATA_NVME | Chip erase error: data NVME | 0xEC0000 | 34 |
SIG_CE_BCUR | Chip erase error: BOCOR, UROW | 0xEC0000 | 35 |
SIG_CE_BC | Chip erase error: BC check | 0xEC0000 | 36 |
SIG_BOOT_OPT | BOOTOPT parameter error | 0xEC0000 | 40 |
SIG_BOOT_ERR | Boot image hash verify fail | 0xEC0000 | 41 |
SIG_BOCOR_HASH | BOCOR hash error | 0xEC0000 | 42 |
SIG_CRC_BADTBL | Bad CRC table | 0xEC0000 | 50 |
SIG_SECEN0_ERR | PAC or IDAU cfg check failure | 0xEC0000 | 60 |
SIG_SECEN1_ERR | PAC or IDAU cfg check failure | 0xEC0000 | 61 |
SIG_EXIT_ERR | Exit: BC or check error | 0xEC0000 | 70 |
SIG_HARDFAULT | Hardfault error | 0xEC0000 | F0 |
SIG_BOOTOK | Boot ROM ok to exit | 0xEC0000 | 39 |
CPU Park mode
This mode allows the debugger to get access to the resources of the device during Boot ROM execution while the CPU is trapped in a while loop. The debug access level when entering that mode corresponds to the DAL value which is programmed in the device.
This mode is reached by sending the Exit command (CMD_EXIT) without clearing the DSU.STATUSA.BREXT bit to the Boot ROM.
As soon as the BREXT bit is cleared, the device exits this state and performs a system reset.
At this point, the MPU is still enabled and prevents software execution elsewhere than in Boot ROM region.
If the host needs to run software on the device, MPU must be disabled by accessing the Cortex-M23 MPU CTRL register with the debugger.