20.6.5.2.5 Accuracy

There are three main factors that determine the accuracy of Fclkdfll48m. These can be tuned to obtain maximum accuracy when fine lock is achieved.

  • Fine resolution. The frequency step between two Fine values. This is relatively smaller for higher output frequencies.
  • Resolution of the measurement: If the resolution of the measured Fclkdfll48m is low, i.e., the ratio between the CLK_DFLL48M frequency and the GCLK_DFLL48M frequency is small, the DFLL48M might lock at a frequency that is lower than the targeted frequency. It is recommended to use a reference clock frequency of 32.768 kHz or lower to avoid this issue for low target frequencies.
  • The accuracy of the reference clock.