47.6.5 Configuring the Operational Amplifiers

Each individual operational amplifier is configured by its respective Operational Amplifier Control x register (OPAMPCTRLx). These settings must be configured before the amplifier is started.

  • Select the positive input in OPAMPCTRLx.MUXPOS
  • Select the negative input in OPAMPCTRLx.MUXNEG
  • Select RES1EN if resistor ladder is used
  • Select the input for the resistor ladder in OPAMPCTRLx.RES1MUX
  • Select the potentiometer selection of the resistor ladder in OPAMPCTRLx.POTMUX
  • Select the VCC input for the resistor ladder in OPAMPCTRLx.RES2VCC
  • Connect the operational amplifier output to the resistor ladder using OPAMPCTRLx.RES2OUT
  • Select the trade-off between speed and energy consumption in OPAMPCTRLx.BIAS