5.6.9 Command Complete Event
| Event | Event Code | Event Parameters |
|---|---|---|
Command_Complete | 0X0E | Num_HCI_Command_Packets Command_Opcode Return_Parameters |
Use this event to transmit the return status of a command and the other event parameters that are specified for the issued HCI command. The Num_HCI_Command_Packets event parameter allows the controller to indicate the number of HCI command packets the host can send to the controller. The event parameters are shown in the following figure.
| Command | Size | Value | Parameter Description |
|---|---|---|---|
Num_HCI_Command_Packets | 1 octet | 0xXX | The Number of HCI Command packets which are allowed to be sent to the Controller from the Host. Range: 0 to 255 |
Command_Opcode | 2 octets | 0x0000 | No associated command |
| 0xXXXX | (non-zero) Opcode of the command that caused this event | ||
Return_Parameter(s) | Depends on command | 0xXX | This is the return parameter(s) for the command specified in the Command_Opcode event parameter. See each command’s definition for the list of return parameters associated with that command |
| Item | Firmware Version 1.0 and Later | Description |
|---|---|---|
| Example: | 04 0E 04 01 7B 20 00 | Command complete event with status parameter |