5.3.4.1 Set Central Initial Connection Parameter or Set Initial Connection Parameter

Table 5-40. Format
Firmware Version 1.0Firmware Version 1.2 and Later
ST,<hex16>,<hex16>,<hex16>,<hex16>

SICP,<hex16>,<hex16>,<hex16>,<hex16>

Note: All firmware version 1.0 syntax remains valid in version 1.2 and later.

This command sets the initial connection parameters of the central device for future connections. This command expects four input parameters, and all are 16-bit values in hex format. For any modifications in current connection parameters, refer to Request Connection Parameter Update or Update Connection Parameter.

The corresponding get command, GT or GICP, returns the desirable connection parameters set by command ST or SICP when the connection is not established. When the connection is established, the actual connection parameters display in response to command GT or GICP.

Connection interval, latency and timeout are often associated with how frequently a peripheral device must communicate with the central device and are , therefore, closely related to power consumption. The following table provides details about the parameters, range and description.

The connection parameters need to adhere to the following rules.

Latency <= 30

Maximum Interval×1.25×(1+Latency)4Seconds,(4Seconds=400ms)
Maximum Interval×1.25ms×(1+Latency)×5<Timeout×10ms
Table 5-41. Connection Parameters

Parameter

Range

Description

Minimum interval

0x0006-0x0C80

  • The minimum time interval of communication between two connected devices
  • Unit – 1.25 ms

Maximum interval

0x0006-0x0C80

  • The maximum time interval of communication between two connected devices
  • Unit – 1.25 ms; must be larger or equal to minimum interval

Latency

0x0000-0x01F3

Must be less than ((Timeout*10/Inter- val*1.25)-1)

The maximum number of consecutive connection events. The peripheral device is not required to communicate with the central device.

Timeout

0x000A-0x0C80

  • The maximum time allowed between raw communications before the link is considered lost
  • Unit – 10 ms
ItemFirmware Version 1.0 and LaterDescription
Default:0010, 0010, 0000, 0048
Example:ST,0020,0064,0002,0064

Set the interval between 40-125 ms, latency to 2 events and timeout to 1s

Response:AOKSuccess
ErrSyntax error or invalid parameter
Note: The PDS stores these parameters. The parameters are effective immediately. Apple® iOS® devices have some special requirements for these parameters. The connection parameter update may be rejected if it does not comply with the rules. For more information, refer to the Accessory Design Guidelines on the Apple developer website.

ItemFirmware Version 1.2 and LaterDescription
Default:0010, 0010, 0000, 0048
Example:SICP,0020,0064,0002,0064

Set the interval between 40-125 ms, latency to 2 events and timeout to 1s

Response:AOKSuccess
ErrSyntax error or invalid parameter
Note: The PDS stores these parameters. The parameters are effective immediately. Apple® iOS® devices have some special requirements for these parameters. The connection parameter update may be rejected if it does not comply with the rules. For more information, refer to the Accessory Design Guidelines on the Apple developer website.