5.5.5 Set Event Indication Mask
| Firmware Version 1.0 | Firmware Version 1.2 and Later |
|---|---|
|
|
Note: All firmware version 1.0 syntax remains valid in version 1.2 and later. | |
The RNBD350 module activates one GPIO_PIN_RA3 pin to indicate that there are some changes in the monitoring indicators. When the MCU detects the changes in the GPIO, the MCU sends a command to read what indicators the change included. Therefore, the MCU can send further commands to read the corresponding indicator status. The EIM or SEIM command masks events that target monitoring.
Use the 2-bytes bit mask parameter to set monitoring indicators (see the following table).
|
Bit Index |
Function |
|---|---|
1 | Link quality (RSSI) |
Others | Reserved |
| Item | Firmware Version 1.0 and Later | Description |
|---|---|---|
| Example: | EIM,0002 | Set Event mask enable link quality |
| Response: | AOK | Success |
Err | Syntax error or invalid parameter | |
Note: The PDS stores these parameters. The parameters are effective immediately without a reboot. | ||
| Item | Firmware Version 1.2 and Later | Description |
|---|---|---|
| Example: | SEIM,0002 | Set Event mask enable link quality |
| Response: | AOK | Success |
Err | Syntax error or invalid parameter | |
Note: The PDS stores these parameters. The parameters are effective immediately without a reboot. | ||