5.5.11 Set PMU Mode

Format: SPMU,<0,1>

This command is used to set the PMU mode as MLDO mode or BUCK PWM mode. There is one parameter, which is ‘0’ or ‘1’.
  • 0’ – To select MLDO mode
  • 1’ – To select BUCK PWM mode
The default setting of the RNBD350 module is MLDO mode.
ItemFirmware Version 1.0 and LaterDescription
Default:0
Example:SPMU,1

Set PMU mode as the BUCK PWM mode

Response:AOKSuccess
ErrSyntax error or invalid parameter
Note: The PDS stores this parameter. The parameter is effective after a reboot.