5.3.1.1 Set Device Name with Address or Set Name with Address

Table 5-16. Format
Firmware Version 1.0Firmware Version 1.2 and Later
S-,<text>

SNA,<text>

Note: All firmware version 1.0 syntax remains valid in version 1.2 and later.

This command sets a serialized Bluetooth® name for the device, where <text> is up to 15 alphanumeric characters. This command automatically appends the last two bytes of the Bluetooth MAC address along with _ (underscore) to the name, which is useful for generating a custom name with unique numbering. This command does not have a corresponding get command.

ItemFirmware Version 1.0 and LaterDescription
Default:N/A
Example:S-,MyDeviceSet the device name to MyDevice_XXXX
Response:AOKSuccess
ErrSyntax error or invalid parameter
Note: This parameter is stored in PDS and is effective after restarting advertisement.
ItemFirmware Version 1.2 and LaterDescription
Default:N/A
Example:SNA,MyDeviceSet the device name to MyDevice_XXXX
Response:AOKSuccess
ErrSyntax error or invalid parameter
Note: This parameter is stored in PDS and is effective after restarting advertisement.