3.3.8.5 NVMCTRL_RegionUnlock
Unlocks a NVM region.
This function unlocks a region that was locked using the NVMCTRL_RegionLock() function. The address parameter can be any address within the region. Unlocking a region unlocks all pages in the region and makes these pages accessible to write and erase operations.
void
NVMCTRL_RegionUnlock
(
unit32_t address
);
Precondition
- Validate if NVM controller is ready to accept new request by calling NVMCTRL_IsBusy();
Parameters
- address - Any address in the region to be unlocked
Returns
- void