3.1.1.3 DIAG_COMMON_SFRWriteRead

Returns the status of the SFR_WRITE_READ diagnostic

DIAG_TEST_STATUS 
DIAG_COMMON_SFRWriteRead
( 
    const SFR_PERIPH_TEST_DEF* periph,
    uint32_t* results, 
    uint32_t results_size, 
    bool dump_regs 
);

Operating Mode

  • Function can run at POST and OnDemand if the peripheral is not currently used.
Precondition
  • none

Parameters

  • periph - pointer to structure specifying the test to be run
  • reg_results - optional array of results
  • results_size - size of results array
  • dump_regs

Returns

  • DIAG_TEST_PASSED if no faults were found, otherwise, DIAG_TEST_FAILED.