3.3.13.4 SERCOMx_USART_ReadCallbackRegister
Sets the pointer to the function (and it's context) to be called when the given USART's read events occur.
This function sets the pointer to a client function to be called "back" when the given USART's read events occur. It also passes a context value (usually a pointer to a context structure) that is passed into the function when it is called.
void
SERCOMx_USART_ReadCallbackRegister
(
SERCOM_USART_CALLBACK callback,
uintptr_t context
);
Precondition
- SERCOMx_USART_Initialize must have been called for the associated USART instance.
Parameters
- callback - registered call back function
- context - callers context
Returns
- void