2.5 Get Code Examples from MPLAB Discover
MPLAB Discover bundles available resources from multiple sources into one portal, such as code examples, data sheets, evaluation boards, videos, and blogs.
Web page: MPLAB Discover
Code Examples
Code examples for devices in the PIC32CM family can be found by searching for the device name, e.g., PIC32CM6408PL10048, in the search bar.
Users can download code examples as a .zip file directly from MPLAB
Discover. Repositories ending with “mplab-mcc” can be opened in MPLAB X.
When a code example is hosted on GitHub, MPLAB Discover provides an “Open with GitHub” link. Download the example code from there or use the Git tool on the PC to create a local repository clone.