26.9.1 SSPxSTAT
Note:
- This bit is cleared on Reset and when SSPEN is cleared.
- In I2C Slave mode this bit holds the R/W bit information following the last address match. This bit is only valid from the address match to the next Start bit, Stop bit or not ACK bit.
- ORing this bit with SEN, RSEN, PEN, RCEN or ACKEN will indicate if the MSSP is in Active mode.
- Polarity of clock state is set by the CKP bit.
- I2C receive status does not include ACK and Stop bits.
Name: | SSPxSTAT |
Offset: | 0xF95,0xE95 |
Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | |
SMP | CKE | D/A | P | S | R/W | UA | BF | ||
Access | R/W | R/W | RO | RO | RO | RO | RO | RO | |
Reset | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
Bit 7 – SMP Slew Rate Control bit
Value | Name | Description |
---|---|---|
1 |
SPI Master | Input data is sampled at the end of data output time |
0 |
SPI Master | Input data is sampled at the middle of data output time |
0 |
SPI Slave | Keep this bit cleared in SPI Slave mode |
1 |
I2C | Slew rate control is disabled for Standard Speed mode (100 kHz and 1 MHz) |
0 |
I2C | Slew rate control is enabled for High-Speed mode (400 kHz) |
Bit 6 – CKE
SPI: Clock select bit(4) I2C: SMBus Select bit
Value | Name | Description |
---|---|---|
1 |
SPI | Transmit occurs on the transition from active to Idle clock state |
0 |
SPI | Transmit occurs on the transition from Idle to active clock state |
1 |
I2C | Enables SMBus-specific inputs |
0 |
I2C | Disables SMBus-specific inputs |
Bit 5 – D/A
Data/Address bit
Value | Name | Description |
---|---|---|
x |
SPI or I2C Master | Reserved |
1 |
I2C Slave |
Indicates that the last byte received or transmitted was data |
0 |
I2C Slave |
Indicates that the last byte received or transmitted was address |
Bit 4 – P
Stop bit(1)
Value | Name | Description |
---|---|---|
x |
SPI | Reserved |
1 |
I2C | Stop bit was detected last |
0 |
I2C | Stop bit was not detected last |
Bit 3 – S
Start bit(1)
Value | Name | Description |
---|---|---|
x |
SPI | Reserved |
1 |
I2C | Start bit was detected last |
0 |
I2C | Start bit was not detected last |
Bit 2 – R/W
Read/Write Information bit(2,3)
Value | Name | Description |
---|---|---|
x |
SPI | Reserved |
1 |
I2C Slave | Read |
0 |
I2C Slave | Write |
1 |
I2C Master | Transmit is in progress |
0 |
I2C Master | Transmit is not in progress |
Bit 1 – UA Update Address bit (10-Bit Slave mode only)
Value | Name | Description |
---|---|---|
x |
All other modes | Reserved |
1 |
I2C 10-bit Slave | Indicates that the user needs to update the address in the SSPxADD register |
0 |
I2C 10-bit Slave | Address does not need to be updated |
Bit 0 – BF
Buffer Full Status bit(5)
Value | Name | Description |
---|---|---|
1 |
I2C Transmit | Character written to SSPxBUF has not been sent |
0 |
I2C Transmit | SSPxBUF is ready for next character |
1 |
SPI and I2C Receive | Received character in SSPxBUF has not been read |
0 |
SPI and I2C Receive | Received character in SSPxBUF has been read |