32.2.6 Auto-Conversion Trigger
The auto-conversion trigger allows periodic ADC measurements without software intervention. When a rising edge of the selected source occurs, the ADGO bit is set by hardware.
The auto-conversion trigger source is selected with the ADACT bits.
Using the auto-conversion trigger does not assure proper ADC timing. It is the user’s responsibility to ensure that the ADC timing requirements are met. See the following table for auto-conversion sources.
| ADACT | Auto-conversioin Trigger Source | 
|---|---|
11111 | Software write to ADPCH | 
11110 | Reserved, do not use | 
11101 | Software read of ADRESH | 
11100 | Software read of ADERRH | 
10000 to
                                                  11011 | Reserved, do not use | 
01111 | Interrupt-on-change Interrupt Flag | 
01110 | C2_out | 
01101 | C1_out | 
01100 | PWM4_out | 
01011 | PWM3_out | 
01010 | CCP2_trigger | 
01001 | CCP1_trigger | 
01000 | TMR6_postscaled | 
00111 | TMR5_overflow | 
00110 | TMR4_postscaled | 
00101 | TMR3_overflow | 
00100 | TMR2_postscaled | 
00011 | TMR1_overflow | 
00010 | TMR0_overflow | 
00001 | Pin selected by ADACTPPS | 
00000 | External Trigger Disabled |