13 Regulatory Approval
The ATSAMR30M18A has received the regulatory approval from the following countries:
- United States/FCC ID: 2ADHKR30M
- Canada
- IC: 20266-R30M
- HVIN: ATSAMR30M18A
- PMN: ATSAMR30M18A
- Europe - CE
For USA/Canada, the module has been certified for the modulation modes listed below. The user
must ensure that the module will only work on the 902-928 MHz frequency band and with one of
the modulation modes listed below, when used in USA and Canada. The host product manufacturer must ensure that the RF behavior adheres to the
certification (e.g. FCC, ISED) requirements when the module is installed in the final host
product.
For Europe, the module has been certified for the modulation modes listed below.
The user must ensure that the module will only work on the 868-868.6 MHz frequency band and
with one of the modulation modes listed below, when used in Europe. For
OQPSK-SIN-RC-100/200/400 modes, the maximum certified TX_PWR setting is 9.
- BPSK-20(1)
- OQPSK-SIN-RC-100(1)
- OQPSK-SIN-RC-200
- OQPSK-SIN-RC-400
Note:
- Tests are done for only these modes which are chosen as the worst case modes.
The availability of some specific channels and/or operating frequency bands are country dependent and should be programmed at the Host product factory to match the intended destination. Regulatory bodies prohibit exposing the settings to the end user. This requirement needs to be taken care of via Host implementation.