Perform the following steps for the demonstration of the Bluetooth RF RX mode:
Set up the connection between the
PIC32-BZ6 Curiosity Board and PC. For more
details, refer to Getting Started with MCHPRT3.
In the RF BT tab, perform
the following steps:
From the “RF mode”
drop-down list, select RX Mode.
From the “Channel”
drop-down list, select 2402 MHz for channel 37.
Click START to receive the
Bluetooth Low Energy packet. The number of received packets is shown in the
drop-down list, “RX Packet”.
Figure 4-8. MCHPRT3PIC32-BZ6 GUI for Bluetooth RF RX Mode
Demonstration
DS50004106B
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.