4.3.1.5 Bluetooth Low Energy Adaptivity Frequency Hopping (AFH) Packet Transmission
Perform the following steps for the demonstration of the Bluetooth Low Energy Adaptivity
Frequency Hopping (AFH) packet transmission:
Set up the connection between the PIC32-BZ6
Curiosity Board and PC. For more details, refer to Getting Started with MCHPRT3.
In the RF BT tab, perform the following steps:
From the “RF mode” drop-down list, select AFH Mode.
From the “Payload” drop-down list, select PRBS9 (default
value).
From the “PHY” drop-down list, select the Data Rate (1M, 2M, S =
2 and S = 8), for example, select PHY 1M.
From the “RF mode” drop-down list, select the Output Power, for
example, select 11 dB.
From the “Packet Length” drop-down list, select the Packet Length
(0-255), for example, 255 (default value).
Click START to transmit the Bluetooth Low Energy packet with adaptivity
frequency hopping.
Figure 4-12. MCHPRT3PIC32-BZ6 GUI for Bluetooth Adaptivity
Frequency Hopping (AFH) TX Test Demonstration
DS50004106B
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.