4.3.1.3 Bluetooth RF CW Tone Test

Perform the following steps for the demonstration of the Bluetooth RF CW tone test:
  1. Set up the connection between the PIC32-BZ6 Curiosity Board and PC. For more details, refer to Getting Started with MCHPRT3.
  2. In the RF BT tab, perform the following steps:
    • From the “RF Modes” drop-down list, select CW Mode.
    • From the “Channel” drop-down list, select 2402 MHz for channel 37.
    • From the “Power” drop-down list, select the Output Power, for example, select 11 dB.
  3. Click START to transmit the CW tone at the selected channel.
Figure 4-9. MCHPRT3 PIC32-BZ6 GUI for Bluetooth RF CW Mode Demonstration