5.3.62 _Q16shlNoSat Function
This function shifts a Q16 value by Y bits, to the left if
Y is positive or to the right if Y is negative.
The function sets the _Q16shlSatFlag variable in case of underflow or
overflow but does not take care of saturation.
Include
<libq.h>
Prototype
_Q16 _Q16shlNoSat(_Q16 x, short y);
Arguments
x | a fixed-point number in Q16 format, which ranges from -216 to 216-1. The value of this argument ranges from -2147483648 to 2147483647. |
Y | an integer number, which ranges from -32 to 32. |
Return Value
This function returns the shifted value of x in Q16 format.
The value ranges from -2147483648 to 2147483647.