8.1.4 freeslots
This is a list of slots that may be used by the library when a pkcs11 operation that creates new objects is used. When the library is initialized, it scans for files of the form <pkcs11_slot_num>.<device_slot_num>.conf, which defines the object using that device resource.