15.4.1 Data Structures
The container structure that holds the entire configuration of a binding
layer is given below.
typedef struct qtm_control_tag
{
uint8_t binding_layer_flags;
module_init_t *library_modules_init;
module_proc_t *library_modules_proc;
module_acq_t *library_modules_acq;
module_arg_t *library_module_init_data_model;
module_arg_t *library_module_proc_data_model;
module_arg_t *library_modules_acq_dm;
qtm_acq_pp_t *qtm_acq_pp;
/*******************************/
/* Callbacks for Binding layer */
/*******************************/
qtm_library_init_complete_t qtm_init_complete_callback;
qtm_error_callback_t qtm_error_callback;
qtm_measure_complete_t qtm_measure_complete_callback;
qtm_pre_process_callback_t qtm_pre_process_callback;
qtm_post_process_callback_t qtm_post_process_callback;
} qtm_control_t;| Parameter | Description |
|---|---|
*library_modules_init | Pointer to the array that contains the list of module initialization function pointers |
*library_modules_proc | Pointer to the array that contains the list of module post-processing function pointers |
*library_modules_acq | Pointer to the array that contains the list of acquisition module function pointers |
*library_module_init_data_model | Pointer to the array which contains the Data Pointers of the acquisition modules |
*library_module_proc_data_model | Pointer to the array which contains the Data Pointers of the post-processing modules |
*library_modules_acq_dm | Pointer to the array which contains the pointers of acquisition groups |
qtm_init_complete_callback | Callback provided by binding layer module after executing all the module initializations |
qtm_error_callback | Callback function triggered only if there is any error encountered by the binding layer during the module processes |
qtm_measure_complete_callback | Callback triggered by binding layer module after the completion of measurement and before post-processing |
qtm_pre_process_callback | Callback triggered after the acquisition process and before post processing. This is provided to enable the user to implement custom filtering modules. |
qtm_post_process_callback | Callback triggered by binding layer module after the completion of all the post-processing of modules |