4.2.4 DUT Transmission at High Impedance (CENELEC LISN)
CAUTION: For this part of the
test, the user has to set up Configuration B. See Figure 2-5.
Configure the DUT as the transmitter:
- Select “Transmission” in the DUT instance of the PHY Tester Tool, then click the Next button to continue.
- In the Transmission Parameters
tab:
- Select “Perform EVM and SNR Test” in the transmission parameters setup.
- As DUT is connected in a High Impedance Network, select the branch configuration as “High Impedance”.
- Click the Next button to continue.
Configure the DUT frames (transmitter):
- If the EVM test is checked in the
previous tab, the configuration of the frames is already done with the following
values:
- Time Interval (ms): 100.
- Number of frames: 100.
- Message: [G3|PRIME] IS A GREAT INTEROPERABLE WORLDWIDE TECHNOLOGY, [G3|PRIME] IS A GREAT INTEROPERABLE WORLDWIDE TECHNOLOGY.
- Click the Next button to continue.
- In the last tab, Configuration Summary, check that all values correspond to the desired configuration and wait.
Configure the Reference Board as the receiver:
- Select “Reception” in the Reference instance of the PHY Tester Tool, then click the Next button to continue.
- In the Reception Parameters
tab:
- Select “Perform EVM and SNR Test” in the reception parameters setup.
- Click the Next button to continue.
Configure the reference frames (receiver):
- If the EVM and SNR tests were checked
in the previous tab, the configuration of the frames is already done with the
following values:
- Time Interval (ms): 100.
- Number of frames: 100.
- Message: [G3|PRIME] IS A GREAT INTEROPERABLE WORLDWIDE TECHNOLOGY, [G3|PRIME] IS A GREAT INTEROPERABLE WORLDWIDE TECHNOLOGY.
- Click the Next button to continue.
- In the last tab, Configuration Summary, check that all values correspond to the desired configuration and wait.
Run the test:
- Set an attenuation level of 0 dB.
- Execute the transmission.
- Go to the receiver PHY Tester Tool instance (Reference board in this case), then click the Start Test button.
- Go to the transmitter PHY Tester Tool instance (DUT in this case), then click the Start Test button.
- After that, the test with 0 dB of attenuation starts. Now, the transmission and reception processes are visible in both Test Executions windows. If the messages are different, the receiver will not recognize them as valid. If the configured interval and number of frames are different, the statistics computed at the end of the test may be inaccurate. In both boards’ displays, the transmitted/received messages show.
Store the EVM and SNR results in a spreadsheet:
Tip: Remember to mark the
following information:
DUT operation (TX or RX) + DUT Position (HIGH or LOW) + AttenuationdB
- Copy the table with the EVM and SNR results that appear in the receiver PHY Tester Tool instance (reference board in this case) by clicking the Copy Table button.
- Paste the table in the corresponding
spreadsheet created. Marking information can be
TxHIGH0dB, where:- TX: DUT is operating as transmitter.
- LOW: DUT is connected in High Impedance Network (50R).
- 0 dB: The attenuation between the DUT and the reference is 0 dB.
- The user must repeat the above steps,
varying the attenuation in each process of measurement (0 dB, 10 dB, 20 dB, 30 dB,
40 dB, 50 dB) and updating the spreadsheet with the obtained values. The user will
find some attenuation where the transmission will not be successful.Remember: More attenuation points provide more accurate results.