1.2.3.5 WDRV_PIC32MZW_BSSFIND_NOTIFY_CALLBACK Typedef
typedef bool (*WDRV_PIC32MZW_BSSFIND_NOTIFY_CALLBACK)
C
Summary
Callback to signal discovery of a BSS.
Description
When the information about a discovered BSS is requested the driver will use this callback to provide the BSS information to the user.
Parameters
Param | Description |
handle | Client handle obtained by a call to WDRV_PIC32MZW_Open. |
index | Index of BSS find results. |
ofTotal | Total number of BSS find results. |
pBSSInfo | Pointer to BSS information structure. |
Returns
If true is returned the PIC32MZW driver will automatically fetch the next BSS find results which will cause a later call to this callback. If false is returned the PIC32MZW driver will not fetch the next BSS find results, the user must call WDRV_PIC32MZW_BSSFindNext to retrieve them.
Remarks
The callback function must return true or false. true indicates that the user wishes the next BSS information structure be provided. false indicates that the user will call WDRV_PIC32MZW_BSSFindNext to obtain the next BBS information structure.